This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530CUS Design

Expert 1070 points


I just recieved a board we designed from fabriacation using the OMAP3530CUS (0.6mm pitch) processor.  I can connect to the

part, read and set internal memory, etc.  I can single step the internal ROM code.  However, when I free run the processor,

I get the following message from Code Composer via the JTAG interface:

 

A reset occured on the target.

 

and the "SECURE" indicator flashes on the lower bar of the Code Composer window.  I have looked SYS_nRESPWRON signal to

the processor and don't see any noise or dips.  What other signals are key that could cause the target to reset like this?

 

Thanks.