This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Omap 3530 nSleep trigger?

Hi,

I've got an Omap 3530 with tps 65950. The SYS_OFF_MODE pin of the processor is connected to nSleep1 pin of the tps. Using Linux 2.6.32-rc7 I can see the mpu/core/neon powerdomains are going to off but the power scripts in the tps (sleep script) are not executed. What are the exact conditions for triggering SYS_OFF_MODE? If it is indeed triggered what can cause the tps to ignore the state of nSleep1 pin?

Thanks.