This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

write a jaff2 filesystem on nor flash (DM6446)



Hello,I'd like to place a root filesystem partition into the board NOR  memory.And I have write the u-boot and  linux kernel successfully into the nor flash.The system can be started normally and also can mount the NFS system successfully。 BUT when I login the system and enter the cat  /proc/mtd, HyperTerminal displays only  “dev:    size   erasesize  name". I can not see the Partition information like

"mtd0: 00c00000 00020000 "ROOTFS"
mtd1: 00200000 00020000 "BOOTLOADER"
mtd2: 00200000 00020000 "KERNEL"
mtd3: 03200000 00020000 "NAND ROOTFS partition"
mtd4: 04b00000 00020000 "NAND DATAFS partition"".

My steps as fllowing:

First of all I think this is a kernel configuration issue. My Kernel configuration information about the MTD as fllows:

│<*> Memory Technology Device (MTD) support
│[*] MTD partitioning support
│<*> Direct char device access to MTD devices
<*> Caching block device access to MTD devices
RAM/ROM/Flash chip drivers --->
│<*> Detect flash chips by Common Flash Interface (CFI) probe
│ │<*> Support for Intel/Sharp flash chips
│ │<*> Support for AMD/Fujitsu flash chips

I have made the "ATA/ATAPI/MFM/RLL support" disable.

my nor flash partition information is :

#if defined(CONFIG_MTD) || defined(CONFIG_MTD_MODULE)
// NOR Flash base address set to CS0 by default
#define NOR_FLASH_PHYS 0x02000000

static struct mtd_partition davinci_evm_partitions[] = {

{
.name = "bootloader",
.offset = 0,
.size = SZ_128K,
.mask_flags = MTD_WRITEABLE, // force read-only
},

{
.name = "params",
.offset = MTDPART_OFS_APPEND,
.size = SZ_128K,
.mask_flags = MTD_WRITEABLE,
},

{
.name = "kernel",
.offset = MTDPART_OFS_APPEND,
.size = 0x00300000,
.mask_flags = 0
},

{
.name = "filesystem",
.offset = MTDPART_OFS_APPEND,
.size = MTDPART_SIZ_FULL,
.mask_flags = 0
}
};

static struct physmap_flash_data davinci_evm_flash_data = {
.width = 2,
.parts = davinci_evm_partitions,
.nr_parts = ARRAY_SIZE(davinci_evm_partitions),
};


static struct resource davinci_evm_flash_resource = {
.start = NOR_FLASH_PHYS,
.end = NOR_FLASH_PHYS + SZ_32M - 1,
.flags = IORESOURCE_MEM,
};

static struct platform_device davinci_evm_flash_device = {
.name = "physmap-flash",
.id = 0,
.dev = {
.platform_data = &davinci_evm_flash_data,
},
.num_resources = 1,
.resource = &davinci_evm_flash_resource,
};
#endif

and the information is in the board_evm.c.

 After this I use the commond "make ARCH=arm CROSS_COMPILE=arm_v5t_le- uImage ".And  produceed the the Kernel successfully. I use the JATA write the u-boot and the uImage into the nor flash.

Finally I star the system. Login it .Enter the "cat  /proc/mtd",and the HyperTerminal displays only  “dev:    size   erasesize  name". 

I want to know if I have  missed some steps.I am very confused now.please help me .Thank you very much.