I bought a TMDXICE3359 ICE kit in Dec. 2012 and have been waiting for the Ethernet/IP software to be released. It just came out and I downloaded it. I am using CCS v5.3 and when I started a new project using the Ethernet/IP project in the examples, it did not compile because of missing components related to sys_bios and NDK.
My question is: Is there any documentation or instructions for properly configuring the ICE board to run the new software? The README.txt did not appear to be useful. In looking at the code, there a number of configurable parameters that can be set. Which ones are necessary for the ICE board?
Here are the software components I have downloaded and installed:
CCS v5.3
am335x_sysbios_ind_sdk_win32setup_01_01_00_01.exe
ndk_2_22_03_20.zip
tirtos_setupwin32_1_01_00_25.exe
xdctools_3_24_06_63
I am lost in the minutia -- please help.
BillP