Other Parts Discussed in Thread: OMAP3530
When I run this command: gst-launch -v filesrc location=/spiderMan3.mp4 ! qtdemux name=demux demux.audio_00 ! queue max-size-buffers=8000 max-size-time=0 max-size-bytes=0 ! TIAuddec1 ! alsasink demux.video_00 ! queue ! TIViddec2 ! TIDmaiVideoSink videoStd=D1_PAL videoOutput=COMPOSITE
it shows this error
____________________________________________________________
<3>CMEMK Error: Failed to find a pool which fits 829440
CMEMK Error: Failed to find a pool which fits 829440
CMEM Error: getPool: Failed to get a pool fitting a size 829440
Failed to allocate memory.
ERROR: from element /GstPipeline:pipeline0/GstTIViddec2:tividdec20: failed to re-partition decode buffers after processingfe
_____________________________________________________
I use cat to check cmem module as follow.
[root@HUALU omap3530]# cat /proc/cmem
Block 0: Pool 0: 1 bufs size 5251072 (5250000 requested)
Pool 0 busy bufs:
Pool 0 free bufs:
id 0: phys addr 0x86dfe000
Block 0: Pool 1: 6 bufs size 831488 (829440 requested)
Pool 1 busy bufs:
Pool 1 free bufs:
id 0: phys addr 0x86d33000
id 1: phys addr 0x86c68000
id 2: phys addr 0x86b9d000
id 3: phys addr 0x86ad2000
id 4: phys addr 0x86a07000
id 5: phys addr 0x8693c000
Block 0: Pool 2: 1 bufs size 348160 (345600 requested)
Pool 2 busy bufs:
Pool 2 free bufs:
id 0: phys addr 0x868e7000
Block 0: Pool 3: 1 bufs size 4096 (1 requested)
Pool 3 busy bufs:
Pool 3 free bufs:
id 0: phys addr 0x868e6000
But I can play avi file. I played mp4 file successful once time.
my bootargs is setenv bootargs 'mem=99M console=ttyS2,115200n8 console=ttyS0 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootdelay=1 omap-dss.def_disp="hdmi" omap_vout.vid1_static_vrfb_alloc=y omap_vout.video1_numbuffers=3 omap_vout.video1_bufsize=829440 omap_vout.video2_numbuffers=0'
what is wrong ?