Hi,
I have installed C6678LE EVM on Intel core i3 PC running Ubuntu 12.04. When I boot my PC, the PC does not detect the PCIe card. Even the ehternet of PC is not getting enabled. I tried to program the IBL as said in wiki page (http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide#IBL). But still I see the same issue. I am using AMC to PCIe adapter (TMDXEVMPCI)
If I connect the same card to an Core 2 Duo machine, the PC is able to detect the PCIe card.
Is there any limitation on the board with respect to Linux OS and motherboard or PC processor?
Regards,
Sri.