I am attempting to run an application from flash that was converted from DSP to SYS/BIOS, and have so far only maintained all legacy code.
In my linker.cmd file, there is section designation "Codestart" to "BEGIN_FLASH" at 0x33fff6, however, when I add:
- var Boot = xdc.useModule('ti.catalog.c2800.init.Boot');
- Boot.bootFromFlash = true;
 
 
to the cfg file, there is no designation for this.  I've read that placing this in the cfg file add the branch to c_init00 at the BEGIN section, but since mine was named BEGIN_FLASH I wasn't sure if it didn't know where to put it.  Since I only have 0x2 bits, there is only room for one of these, and since they are essentially the same thing, I don't know which one to use.
Also, if I let Codestart build without a sections defenition and try to debug the program, my ROV gives the error:
  "Target memory read failed at: 0a30d0040, langth:4 This read is at an INVALID adress according to the applications section map. The application is likely either uninitialized or corrupt."
which is confusing, because my memory map appears as the following, and I'm not sure what is causing the jump to that location.
UTPUT FILE NAME:   <Semikron_SYSBIOS.out>
ENTRY POINT SYMBOL: "_c_int00"  address: 00305452
MEMORY CONFIGURATION
         name            origin    length      used     unused   attr    fill
----------------------  --------  ---------  --------  --------  ----  --------
PAGE 0:
  L01SARAM              00008000   00002000  00001eab  00000155  RW X
  FLASH                 00300000   0003ff80  0000f2be  00030cc2  RW X
  CSM_RSVD              0033ff80   00000076  00000076  00000000  RW X
  BEGIN_FLASH           0033fff6   00000002  00000002  00000000  RW X
  PASSWORDS             0033fff8   00000008  00000008  00000000  RW X
  OTP                   00380400   00000400  00000000  00000400  RW X
  BOOTROM               003fe000   00001fc0  00000000  00001fc0  RW X
PAGE 1:
  MSARAM                00000000   00000800  00000522  000002de  RW X
  DEV_EMU               00000880   00000180  000000d0  000000b0  RWIX
  FLASH_REGS            00000a80   00000060  00000008  00000058  RWIX
  CSM                   00000ae0   00000010  00000010  00000000  RWIX
  ADC_MIRROR            00000b00   00000010  00000010  00000000  RWIX
  XINTF                 00000b20   00000020  0000001e  00000002  RWIX
  CPU_TIMER0            00000c00   00000008  00000008  00000000  RWIX
  CPU_TIMER1            00000c08   00000008  00000008  00000000  RWIX
  CPU_TIMER2            00000c10   00000008  00000008  00000000  RWIX
  PIE_CTRL              00000ce0   00000020  0000001a  00000006  RWIX
  PIEVECT               00000d00   00000100  00000000  00000100  RW X
  DMA                   00001000   00000200  000000e0  00000120  RWIX
  MCBSPA                00005000   00000040  00000025  0000001b  RWIX
  MCBSPB                00005040   00000040  00000025  0000001b  RWIX
  ECANA                 00006000   00000040  00000034  0000000c  RWIX
  ECANA_LAM             00006040   00000040  00000040  00000000  RWIX
  ECANA_MOTS            00006080   00000040  00000040  00000000  RWIX
  ECANA_MOTO            000060c0   00000040  00000040  00000000  RWIX
  ECANA_MBOX            00006100   00000100  00000100  00000000  RWIX
  ECANB                 00006200   00000040  00000034  0000000c  RWIX
  ECANB_LAM             00006240   00000040  00000040  00000000  RWIX
  ECANB_MOTS            00006280   00000040  00000040  00000000  RWIX
  ECANB_MOTO            000062c0   00000040  00000040  00000000  RWIX
  ECANB_MBOX            00006300   00000100  00000100  00000000  RWIX
  EPWM1                 00006800   00000022  00000022  00000000  RWIX
  EPWM2                 00006840   00000022  00000022  00000000  RWIX
  EPWM3                 00006880   00000022  00000022  00000000  RWIX
  EPWM4                 000068c0   00000022  00000022  00000000  RWIX
  EPWM5                 00006900   00000022  00000022  00000000  RWIX
  EPWM6                 00006940   00000022  00000022  00000000  RWIX
  ECAP1                 00006a00   00000020  00000020  00000000  RWIX
  ECAP2                 00006a20   00000020  00000020  00000000  RWIX
  ECAP3                 00006a40   00000020  00000020  00000000  RWIX
  ECAP4                 00006a60   00000020  00000020  00000000  RWIX
  ECAP5                 00006a80   00000020  00000020  00000000  RWIX
  ECAP6                 00006aa0   00000020  00000020  00000000  RWIX
  EQEP1                 00006b00   00000040  00000040  00000000  RWIX
  EQEP2                 00006b40   00000040  00000040  00000000  RWIX
  GPIOCTRL              00006f80   00000040  0000002e  00000012  RWIX
  GPIODAT               00006fc0   00000020  00000020  00000000  RWIX
  GPIOINT               00006fe0   00000020  0000000a  00000016  RWIX
  SYSTEM                00007010   00000020  00000020  00000000  RWIX
  SPIA                  00007040   00000010  00000010  00000000  RWIX
  SCIA                  00007050   00000010  00000010  00000000  RWIX
  XINTRUPT              00007070   00000010  00000010  00000000  RWIX
  ADC                   00007100   00000020  0000001e  00000002  RWIX
  SCIB                  00007750   00000010  00000010  00000000  RWIX
  SCIC                  00007770   00000010  00000010  00000000  RWIX
  I2CA                  00007900   00000040  00000022  0000001e  RWIX
  L27SARAM              0000a000   00006000  0000487a  00001786  RW X
  SRAM                  00200000   00020000  00001903  0001e6fd  RW X
  PARTID                00380090   00000001  00000001  00000000  RWIX
  CSM_PWL               003f7ff8   00000008  00000008  00000000  RWIX