Hi there,
im playing around with the WiFi-Display tool which streams the display of a device to another device and ran into a problem. My hardware platform is a TI OMAP5 5432 uEVM ES2.0 (Panda5) board. My software platform is a Omappedia release http://omapedia.org/wiki/Panda5AJ.1.5_Release_Notes (Android 4.2 with a 3.4 Kernel).
I have two EVM boards and connect them via Ethernet. I start the wfd tools via "wfd -l ip:port" and one with "wfd -c ip:port". Both connect to each other and exchange some RTSP meta data. When it comes to streaming, the server's kernel panics and the whole device reboots. I think it has something to do with the writeback pipeline. I tried the same with OMAP4 hardware (same OS, android 4.2 with kernel 3.4) and had the same results. So i dont think its a hardware issue.
My question is: Has anyone here used the wfd tools successfully? Which software release did you use. Which hardware plattform did you use?6303.wfd_receiver.txt4745.wfd_sender.txt4137.wfd_sender_kernelpanic.txt I'll attach my logcat and kernel messages to this posting.
Thanx in advance and kind regards,
Christian