Hi
Referring to the TI HUA Wiki page:
http://processors.wiki.ti.com/index.php/MCSDK_HUA_Demonstration_Guide
we have the following questions:
1) Can we run HUA loopback task with UDP packets and use iperf on a WinXP test machine? if so, should we run one instance of iperf, in client mode?
2) If that's not possible, can we run the Transmit test and use iperf on the WinXP machine to listen to UDP packets?
Currently we just need to measure functionality and not throughput. We are using the DSPC8681 PCIe card and it's taken a long time (4 weeks) to get the HUA project patched and rebuilt for this card and to the point of running - so for now, just seeing UDP packet flow would be a big step.
Srinivasalu
-Signalogic