Hi,
I'm working with the OMAP3530 processor, I'm using the source code of Beagle board as a reference code. In the Linux driver source code for the beagle board, there is code for the highspeed MMC controller( omap_hsmmc.c) , which controls two MMC cards.
In our board also we do want to support two MMC cards. I want to know, can I use the code as such for controlling the two MMC cards, or Do I want to change the file(omap_hsmmc.c) for controlling the two MMC cards.
Awaiting for reply and comments.
Regards,
Devakumar J