Other Parts Discussed in Thread: CCSTUDIO, OMAP3530
Hi all,
I am using a Mistral omap 35x EVM board, and a XDS510USB JTAG emulator (from Digital Spectrum).
When I try to configure the board in "CCStudio Setup", using the specific configuration
for the mistral board (which is included with the XDS510USB drivers), it gives an error:
"Error automatically generating board file. An invalid router family was specified".
It seems as if CCStudio setup doesn´t like the CS_DAP_PC router.
I´ve tried the configuration files for other boards with omap 3530, but all of them use internally the same values,
and give that same error.
Has anybody found that same problem? any suggestion?
Any known workaround?
Thank you very much,
Jose.
P.D: The CCStudio version is v3.3. and the emullator drivers are "setupCCSPlatinum_v30327A"
(downloaded from Spectrum Digital webpage)