Other Parts Discussed in Thread: OMAP3530, TVP5146
Hi All,
We have an issue in OMAP3530 ISP driver on kernel
2.6.22. We are using MT9V023 sensor to capture the video and display
it on LCD. The video image on LCD is getting split after a 2 or 3 hrs
run, or if there is any external disturbance. If the mobile phone which
is kept nearer to camera, receives the call / SMS, the video is
getting split.
Following is our observation:
If the camera is working fine, without any split screen, we receive 4 interrupts – in the ISP handler.
isp: irqstatus = 0x02000100 - Overflow Error, VD0 Done
isp: irqstatus = 0x02160000 - Overflow Error, Preview Done, LSC Done, LSC Pre-fetch Completed
isp: irqstatus = 0x03000000 - Overflow Error, Resize done
isp: irqstatus = 0x02000200 - Overflow Error, VD1 Done
Whenever we see the image split issue, we see an additional interrupt.
isp: irqstatus = 0x02080100 - Overflow Error, LSC pre-fetch error
isp: irqstatus = 0x82060000 - H-Sync, Overflow Error, LSC done, pre-fetch completed
isp: irqstatus = 0x02000200 - Overflow Error and VD1 done
isp: irqstatus = 0x02100000 - Overflow Error and Preview done
isp: irqstatus = 0x03000000 - Overflow Error and Resize done
How
to recover/avoid this image spilt issue? Are there any patch for ISP on
2.6.22 kernel?. Can anybody please help us or suggest to fix this
issue? is there any patch to fix this issue?
Thanks
Senthil