Other Parts Discussed in Thread: AM3358
Developing a custom board with the AM3358 connected to a Marvell 88E1310 PHY using the RGMII2 interface. We are using a WINCE700 BSP and the CPSW3GKitl device driver.
We are unable to transmit any frames (EBOOT cannot DHCP an IP address), I can see that RGMII2_TCLK is correct on the scope but RGMII2_TCTL is never asserted. We are configuring in the following way:
1: XLoader is configuring GMII_SEL to 0x3B -> Port 1 not used, Port 2 used for RGMII, not internal delay.
2: EBoot is configuring the pads GPMC_A0:11 to mode 2 -> RGMII2
3: The CPSW3G initialization is per the CPSW3GKitl device driver, and I've checked this follows the instructions in the spruh73g technical manual.
4: On a transmit frame it seems to be doing the correct thing, but when the packet address is written to the DMAHDP register nothing happens (RGMII2_TCTL stays low)
My questions is have we missed any obvious configuration steps relating to enabling RGMII 2?
Also am I correct in thinking the CPSW_P2 registers are for the RGMII2 interface?
I've logged the contents of some registers during a SendFrame and copied this below (it does not look like the stats register is logging any activity).
Any guidance would be appreciated,
Stuart
-- Dump of registers during a SendFrame.
+Cpsw3gSendFrame
Packet is at 0x8FEB4FE8 tx_bd=0xAF0C0600
Copying 590 bytes from 0x8FEB4FE8 to 0xAF0C0000
BuffPtr[0xAF0C0604] set to 0x8F0C0000
BuffOffsetLength[0xAF0C0608] set to 0x0000024E
BuffFlagPktLen[0xAF0C060C] set to 0x0000024E
BuffFlagPktLen[0xAF0C060C] set to 0xE011024E
Writing 0xB0500A00 with 0x8F0C0600 {Physical Address}
CPMAC_A_TX_DMAHDP(KITL_CHANNEL)[0xB0500A00]=0x8F0C0600
RGMII_CTL:
RGMII_CTL[0xB0501288]=0x00000030
TX_CTL:
CPDMA_TX_CTRL[0xB0500804]=0x00000001
STATS REG:
STATS_GOOD_TX_FRAMES[0xB0500934]=0x00000000
STATS_BCAST_TX_FRAMES[0xB0500938]=0x00000000
STATS_PAUSE_TX_FRAMES[0xB0500940]=0x00000000
STATS_DEFERRED_TX_FRAMES[0xB0500944]=0x00000000
STATS_TX_UNDERRUN[0xB050095C]=0x00000000
STATS_TX_OCTETS[0xB0500964]=0x00000000
ALE:
CPALE_VER_ID[0xB0500D00]=0x00290104
CPALE_CTRL[0xB0500D08]=0x80000000
CPALE_PRESCALE[0xB0500D10]=0x00000000
CPALE_UNK_VLAN[0xB0500D18]=0x00000000
CPALE_PORT_CTRL_0[0xB0500D40]=0x00000003
CPALE_PORT_CTRL_1[0xB0500D44]=0x00000013
CPALE_PORT_CTRL_2[0xB0500D48]=0x00000000
CPALE_PORT_CTRL_3[0xB0500D4C]=0x00000000
CPALE_PORT_CTRL_4[0xB0500D50]=0x00000000
CPALE_PORT_CTRL_5[0xB0500D54]=0x00000000
MAC:
CPMAC_MAC_CTRL(1)[0xB0500D84]=0x00000020
CPMAC_MAC_STS(1)[0xB0500D88]=0x80000000
CPMAC_MAC_TX_PAUSE(1)[0xB0500D9C]=0x00000000
PORT:
CPSW_P0_CONTROL[0xB0500100]=0x00000000
CPSW_P0_VLAN[0xB0500114]=0x00000000
CPSW_P1_CONTROL[0xB0500200]=0x00000000
CPSW_P1_VLAN[0xB0500214]=0x00000000
CPSW_P2_CONTROL[0xB0500300]=0x00000000
CPSW_P2_VLAN[0xB0500314]=0x00000000
DMA:
CPDMA_TX_VER_ID[0xB0500800]=0x00180108
CPDMA_TX_CTRL[0xB0500804]=0x00000001
CPDMA_DMA_CTRL[0xB0500820]=0x00000001
CPDMA_DMA_STS[0xB0500824]=0x80000000
-Cpsw3gSendFrame