Other Parts Discussed in Thread: OMAP-L137, OMAP-L138
Hi,
We've problem with using BSL of L138 EVM in DSPLINK (v. 1.63). We tried to make a sample DSPLINK application work with such simple BSL functions like LED_turnOn but without any success (our aim is to use some code from image-sensor BSL test application in the DSPLINK application). Using EVMOMAPL138_init() function makes the application hangs up. After removing init_clocks() call in EVMOMAPL138_init() the "message" DSPLINK application works correctly so I suppose that the problem may be with config_pll0() and config_pll1() calls in init_clocks().
It's been two weeks since we reported the problem to support@ti.com - unfortunately, with no answer.
Any suggestions how to use BSL to access L138 EVM peripherals in DSPLINK application?
Regards
Andrzej