This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Full blast testing / max out power consumption

A question a bit between here, linux and wlan/wilink forums.

I'd like to run some tests to ensure every peripheral of the AM335x is running at it's limit (max current draw).
So,
- full trafic on DDR3
- keep the NEON 100% buzy
- Run ADCs, pwm's, etc 
(in my case) 
- do power-hungry operations on nand
- max out the wilink on max gain

...and so on.
Let me know if I'm missing something. Anything I can do to eat more power is greatly appreciated.

I suspect there could be some handy tools to do this in linux that I'm not aware of. please advice.

thanks /d