Other Parts Discussed in Thread: OMAP-L138, OMAP-L137
Hi all,
is there a way to connect zoom exeperimenters kit for OMAP L-138 to the normal PC display? Like a DVI "extender" or something?
b.r.
OskarM.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Oscar,
There are plans to make an adapter to connect to the OMAP-L138 board based on the design of the adapter for the OMAP-L137:
http://tiexpressdsp.com/index.php/OMAP-L1x_VGA
The hardware and the software to use should be ready beginning of 2010.
There is also a open source board on the way (not a TI board):
http://hawkboard.wordpress.com/