Other Parts Discussed in Thread: TMS320C6748
Hey,
I have an application with (5) external microprocessors that can act like asynchronous FIFOs (similar to Figure 18-9 in the TMS320C6748 DSP technical reference manual). These microprocessors have a chip select, 8-bit data bus, read, and write control lines. I also want to connect a regular asynchronous SRAM to the C6748 (Figure 18-8 a or b). Reading through the technical reference manual, I should be able to connect either kind of device to the C6748. Can I connect both kinds of devices to the C6748 at the same time? Can the DMA read from the FIFO and then write to the ASRAM? I've seen forum posts mentioning using CE space to configure ROMs, SRAMs, etc. at the same time, but I haven't found reference to CE spaces in this particular device.
Thanks,
Tobyn