I am working on funding project of ECG signal processing.
In the proposed work the ECG signal extracted from the body using the general instrumentation is to be processed using the noise removal algorithms, and the signal thus obtained is to be processed with the proposed signal processing techniques to detect the cardiac problems at an early stage. Once suitable technique is identified which provides satisfactory classification of the subjects into control and pathological cases, the technique is to be used in the proposed portable device to be built around a micro controller/DSP.
So, please suggest me a suitable kit for this work. But I can’t decide which one is suitable for my work. The kits are
1. ECG Implementation on the TMS320C5515 EVM.
2. ADS1293 ECG kit
3. ADS4400 SPO2
4. Zoom OMAP-L138 EVM
Can you suggest any one.