Other Parts Discussed in Thread: DM3730, AM3703
I would like to know the idle power consumption for DM3730 system. Although there is a spreadsheet to calculate the DM3730 power consumption, but we could never achieve that number in spreadsheet, using TI Android BSP 2.3.6. Not sure if the spreadsheet is misleading or the BSP is not doing its job properly.
Compared with Motorola DEFY phone (similar architecture from TI, Android 2.3.6 ), DEFY could achieve less than 50mA in idle mode (do not include display)
Using TI BSP, our DM3730 setup could achieve 150mA in the idle mode (Process + DDR+ PMIC, do not include display)
What could be the cause of this huge difference? What should be our reason power target for DM3730 setup?