Other Parts Discussed in Thread: OMAP-L137
I have a problem running CCS 3.3 on the OMAP-L137 EVM board.
I started up CCS 3.3 after booting my board and attempted to connect to the TMS320C674XP_0 device from the Parallel Debug Manager and got the following error message:
I tried the same thing interrupting the boot sequence to get U-Boot control and got the same error message.
Not sure what to try next.
-------------------------------------------------
Error connecting to the target:
Error 0x80000240/-1180
Fatal Error during: Initialization, OCS,
The target is stuck in Wait-in-Reset mode. The applied reset must be released before progressing.
I/O Port = 510
Board Name: EVMOMAP_L137
Cpu Name: TMS320C674XP_0
Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.
------------------------------------------------