A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a customer that has a project with OMAP3530. Regarding the analog video output (VENC) he read that the voltage level are not compliant with NTSC/PAL specified and that many TV has AGC and accept signal below the nominal.
Anyway he want provide a signal compliant with the specification (1.21V with 75ohm termination instead of 0.88V of OMAP output).
He thought to use OPA362, but is specified for OMAP3430 and he want to know also is suitable for OMAP3530.
Furthermore he want some suggestion how to connect the device to the OMAP3530