Dear Sir,
I am new to OMAP4 and android. Our board is pandaboard 4460 and camera sensor is ov5640 MIPI interface.
Camera buy from http://www.e-consystems.com/OMAP4-MIPI-Camera-Board.asp
It's work on ubuntu/linux but faild on android.
Android version is 4.2.2 build from www.linaro.org
camera test log
/system/bin/camera_test -f
openCamera(camera_index=0)
Unable to connect to CameraService
Retrying...
Giving up!!
Camera initialization failed
I have no idea how to modify ducati.
Where can download the pre-built ducati firmware which support pandaboard 4460 with ov5640?
tks .
kuda