This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C66x sRIO Port Link Timeout Configurations



The equations of Port Link Timeout interval as follows:

 - Shortest: SRV_CLK * TIMEOUT_VALUE * 3
 - Longest: SRV_CLK * TIMEOUT_VALUE * 4

 NOTE: The SRV_CLK mean the Prescaled IP_CLK, where the Prescaled IP_CLK period = (IP_CLK period x PRESCALAR_SRV_CLK value).

Why is it that there are two equations, i.e. Shortest and Longest?

For the SP_LT_CTL.TIMEOUT_VALUE Field, in Row of the "value" in the Table 3-80, there are the eight values. Must these values be used?

Serial RapidIO (SRIO) for KeyStone Devices User's Guide (Rev. B)
http://www.ti.com/lit/ug/sprugw1b/sprugw1b.pdf
3.14.18 SP_LT_CTL

Best regards,

Daisuke

 

  • Hi,

    Please give me an answer as soon as possible.
    Your prompt reply would be appreciated.

    Best regards,

    Daisuke

     

  • Hi Daisuke,

    I have found some additional information on this issue. I need to confer with a colleague on my findings and I will provide my feedback here. I will reply in about a day with my input.

    Thanks,

    Clinton

  • Hi Daisuke,

    I wanted to give you an update. I'm still confirming the details of the port link timeout register. It will most likely be a couple days before I have more feedback. I'll post it here once I do.

    Thanks,

    Clinton

  • Hi Daisuke,

    Daisuke Maeda said:
    Why is it that there are two equations, i.e. Shortest and Longest?

    The 2 equations provide a range for the timeout period for a selected timeout value. The actual timeout period for a port can vary between the calculated 'shortest' and 'longest' period.

    Daisuke Maeda said:
    For the SP_LT_CTL.TIMEOUT_VALUE Field, in Row of the "value" in the Table 3-80, there are the eight values. Must these values be used?

    No, you can use any value between 0x000000 and 0xFFFFFF, inclusive. As noted, a value of 0 will disable the timer. I will make sure that the documentation gets updated.

    Please let us know if you have any additional questions or comments.

    Thanks,

    Clinton

  • Daisuke,

    I wanted to add some additional clarification. The actual time for the timeout can vary for each transaction between the calculated 'shortest' and 'longest' values. This is based on how the counter is implemented. This is compliant to the RapidIO standard.

    Thanks,

    Clinton

  • Hi Clinton,

    Thank you for your reply.

    Please let me confirm just in case. Is the actual timeout period to vary for each transaction not user-defined?

    Best regards,

    Daisuke

     

  • Hi Daisuke,

    The timeout period is selected based on the prescaled IP_CLK and the user selected TIMEOUT_VALUE. However, that period can vary between the calculated 'shortest' and 'longest' values.

    Below I have provided an example of the 'shortest' and 'longest' values for the Port Link Timeout interval for a given prescaled IP_CLK configuration. This means that the actual timeout for one transaction could be 0.2976 uS and the next could be 0.3968 uS (or anything in between those 2 values).

    IP_CLK

    Frequency (MHz)

    IP_CLK

    Period (uS)

    RIO_IP_PRESCAL

    Prescaled

    IP_CLK

    period (uS)

    Port Link Timeout

    Shortest (uS)

    Port Link Timeout

    Longest (uS)

    312.5

    0.003

    31

    0.0992

    0.2976

    0.3968

    Let us know if this clarifies things or if you have any further questions.

    Thanks,

    Clinton

  • Hi Clinton,

    Thank you for your reply. I understand.

    Best regards,

    Daisuke