I am looking for the latest version of EVM Flash. I currently have revision 1.2, but I am unable to capture an image of the onboard Micron flash. Here is my debug output from EVM Flash:
Download [08:38:15]: [00] Initiating OMAP ROM code communication
Download [08:38:15]: [00] Opening UART/USB connection
Download [08:38:15]: [00] Waiting for target to reset
Download [08:38:19]: [00] ASIC ID read (0x45 bytes)
Download [08:38:19]: [00] GP device detected.
Download [08:38:19]: [00] Second file read: .\targets\2nd-downloaders\dnld_startup_3530evm_gp.2nd
Download [08:38:19]: [00] Transferring second file to target
Download [08:38:19]: [00] Second file transferred to target (0x5704 bytes)
Download [08:38:19]: [00] Releasing UART/USB connection...
Download [08:38:20]: [00] Reconnecting to target (LL connect)
Download [08:38:20]: [00] Verifying connection
Download [08:38:20]: [00] Connection successfully established
Download [08:38:20]: [00] Processing read to buffer request on device type: 0x2
Download [08:38:20]: [00] Could not locate specified device type (#0x02) at: 0x00000000 in XML file
Download [08:38:20]: [00] Read operation completed. Result = 0xFFFFFFEF
Download [08:38:51]: [00] Initiating OMAP ROM code communication
Download [08:38:51]: [00] Opening UART/USB connection
Download [08:38:51]: [00] Waiting for target to reset
Download [08:38:55]: [00] ASIC ID read (0x45 bytes)
Download [08:38:55]: [00] GP device detected.
Download [08:38:55]: [00] Second file read: .\targets\2nd-downloaders\dnld_startup_3530evm_gp.2nd
Download [08:38:55]: [00] Transferring second file to target
Download [08:38:55]: [00] Second file transferred to target (0x5704 bytes)
Download [08:38:55]: [00] Releasing UART/USB connection...
Download [08:38:56]: [00] Reconnecting to target (LL connect)
Download [08:38:56]: [00] Verifying connection
Download [08:38:56]: [00] Connection successfully established
Download [08:38:56]: [00] Processing read to buffer request on device type: 0x2
Download [08:38:56]: [00] Could not locate specified device type (#0x02) at: 0x00000000 in XML file
Download [08:38:56]: [00] Read operation completed. Result = 0xFFFFFFEF
Am I possibly setting the start and ending addresses wrong?