Other Parts Discussed in Thread: OMAP3530
Hi,
While building the DSP side sample I see
Generating DSP/BIOS configuration files ...
js: "/home/development/ti-sdk-beagleboard-05.07.00.00/xdctools_3_15_00_33/include/utils.tci", line 407: Error: Environment variable 'config.programName'="/home/development/ti-sdk-beagleboard-05.07.00.00/dsplink_linux_1_65_02_09/dsplink/dsp/BUILD/OMAP3530_0/LOOP/BIOS_DEB/loop" contains the character '.', which is not allowed in a program name. Please, select a program name without '.' in its path. See SDOCM00050016 for more information.
INTERNAL ERROR: load added null
make[2]: *** [DspBios/5.XX/OMAP3530/loop_tsk.tcf.deb] Error 1
make[1]: *** [objdeb] Error 2
make: *** [loop.objdeb] Error 2
What will be the possible cause? Kindly help me out from this build process.