Hi folks,
The configuration that I am using has an image sensor connected to the ISS camera input on he DM814x. The sensor is also connected to another device on the board that captures the sensor image too (so effectively there are two paths from the sensor).
What I am seeing is that the video frames captured on the ISS are horizontally offset to the left by approximately 100 pixels. This results in the captured frames losing a column of about 100 pixels wide on the left of the image and gaining a black vertical strip about 100 pixels wide on the right of the image.
It is almost like the horizontal sync signal is arriving too late for the video image. However, capturing an image from the other device on our board that receives the image from the same sensor at the same time shows that the horizontal and vertical sync signals seem to be OK.
I am using ISS software version 3.5 combined with EZSDK 5.05.
Has anyone come across this behaviour before?
Is there any way in software to adjust when an ISS image capture starts?
Thanks in advance,
Regards,
Terry