This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WINCE BSP 6.11 does not output 720P DVI on OMAP3530 EVM

Has any one tested the DVI outputs for the WinCE 6.2 BSP developed by BSQUARE?

Most resolutions on version 6.10 worked well. However, they don't work for version 6.11.

The symptom is that the signals are not recognized by TVs/monitors. The only one resolution recognized by all TVs and monitors is "BSP_DVI_800W_600H".

I noticed the output was recognozed at the EBOOT stage. It became unrecognizable after the kernel was up.

We care about 720P (BSP_DVI_1280W_720H), but it was not recognized by most of our tesing TVs and monitors. The only recognizing TV shows the framerate is 77, instead of 60. It is most probably the reason.

Any one has the same problem and has any idea?

Thanks in advance.

Kevin