I've worked with Martin over in the CCS group to see what was the cause of a CCS freeze I was having, but my main issue now is that I have mailboxes and semaphores defined through the GUI configurator, but during compile time, my C code cannot find the mailbox or semaphore symbols. I'm stymied, as I've followed the tutorial resources on configuration that are available, and nothing appeared incorrect to either myself or Martin. My management is about ready to have my head on a pike as it is taking painfully long to get this resolved. There is probably something very simple that is wrong, but I don't see it and the dearth of troubleshooting and tutorial resources is making this worse. 4721.build log.zip
Incidentally, you can't attach build log files directly as their lack of extension prohibits their upload to TI's system. I had to zip the file because of this