Other Parts Discussed in Thread: OMAP3530
Hi
I have seen snaphots of quake game on the beagle board.
and I am trying to test the quake game on the OMAP3530 based beagle board.
But after including the quake2 in the open embedded package and when executing i am getting the below error,
Please provide some pointers to fix this issue.
Thanks
Robin
root@beagleboard:/usr/bin# ./quake2
Quake 2 -- Version 3.21+r0.16 Debug
using /home/root/.quake2/baseq2/ for writing
couldn't exec default.cfg
couldn't exec config.cfg
Console initialized.
------- sound initialization -------
sound sampling rate: 11025
------------------------------------
------- Loading ref_soft.so -------
LoadLibrary("ref_soft.so") failed: No such file or directory
Refresh failed
recursive shutdown
Error: Couldn't fall back to software refresh!