Other Parts Discussed in Thread: OMAPL138
Brad or anyone in the know:
When is sata going to be implemented in linux for the L138? The linux roadmap on wiki doesn't talk about the sata interface.
Thanks,
TS
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Assuming you are using a hard disk, plug it in along with power to the drive and watch the console messages when it boots. Drive should be identified and appear in the console messages. Once you log in you'll have to mount the drive. I did try a compact flash sata drive but it was not recognized. Use a standard hard disk for initial testing and should work fine. If you don't see the kernel message during boot you'll have to check and see if it is included in the kernel build. I've rebuilt my kernel numerous times and can't remember if it came enable or had to enable and rebuild.
Kev
One other thing forgot is prior to mounting you'll have to partition the drive. Just google it and there are lot's of how-to's using fdisk.
Kev