Hi...
I am trying to boot beaglebone with jellybean and i followed the instructions in the link
http://processors.wiki.ti.com/index.php/TI-Android-JB-4.2.2-DevKit-4.1.1_DeveloperGuide
Everything worked fine..But when i tried to boot the beaglebone from using the jellybean image i got a log message which i pasted below..
Press CTRL-A Z for help on special keys
[ 35.394104] request_suspend_state: wakeup (0->0) at 35361010854 (2000-01-01 00:00:33.584518288 UTC)
U-Boot SPL 2013.01.01-00123-g2830d15 (Oct 01 2013 - 12:29:20)
No AC power, disabling frequency switch
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img
U-Boot 2013.01.01-00123-g2830d15 (Oct 01 2013 - 12:29:20)
I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
NAND: No NAND device found!!!
0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - readenv() failed, using default environment
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw
Hit any key to stop autoboot: 0
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
214 bytes read in 3 ms (69.3 KiB/s)
Loaded environment from uEnv.txt
Importing environment from mmc ...
Running uenvcmd ...
reading uImage
4178848 bytes read in 462 ms (8.6 MiB/s)
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-3.2.0-00244-gcf99001
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 4178784 Bytes = 4 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0-00244-gcf99001 (root@adheeth) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #1 Tue Oct 1 11:19:29 IST 2013
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES1.0 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
[ 0.000000] Kernel command line: console=ttyO0,115200n8 androidboot.console=ttyO0 mem=256M root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait init=/init ip=off
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 256MB = 256MB total
[ 0.000000] Memory: 249984k/249984k available, 12160k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc078a000 (7688 kB)
[ 0.000000] .init : 0xc078a000 - 0xc07e0000 ( 344 kB)
[ 0.000000] .data : 0xc07e0000 - 0xc084ba70 ( 431 kB)
[ 0.000000] .bss : 0xc084ba94 - 0xc09a3890 (1376 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[ 0.118591] pid_max: default: 32768 minimum: 301
[ 0.118743] Security Framework initialized
[ 0.118804] Mount-cache hash table entries: 512
[ 0.119262] CPU: Testing write buffer coherency: ok
[ 0.119323] ftrace: allocating 22068 entries in 65 pages
[ 0.188385] omap_hwmod: pruss: failed to hardreset
[ 0.189270] print_constraints: dummy:
[ 0.189483] NET: Registered protocol family 16
[ 0.190643] OMAP GPIO hardware version 0.1
[ 0.191711] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.192840] omap_i2c.1: alias fck already exists
[ 0.193359] omap2_mcspi.1: alias fck already exists
[ 0.193481] omap2_mcspi.2: alias fck already exists
[ 0.193634] edma.0: alias fck already exists
[ 0.193634] edma.0: alias fck already exists
[ 0.193664] edma.0: alias fck already exists
[ 0.203979] bio: create slab <bio-0> at 0
[ 0.204986] SCSI subsystem initialized
[ 0.205841] usbcore: registered new interface driver usbfs
[ 0.205963] usbcore: registered new interface driver hub
[ 0.206115] usbcore: registered new device driver usb
[ 0.206420] registerd cppi-dma Intr @ IRQ 17
[ 0.206451] Cppi41 Init Done Qmgr-base(d087a000) dma-base(d0878000)
[ 0.206451] Cppi41 Init Done
[ 0.206481] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.206634] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.218627] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.219451] tps65910 1-002d: could not be detected
[ 0.219970] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.220550] Bluetooth: Core ver 2.16
[ 0.220611] NET: Registered protocol family 31
[ 0.220642] Bluetooth: HCI device and connection manager initialized
[ 0.220642] Bluetooth: HCI socket layer initialized
[ 0.220642] Bluetooth: L2CAP socket layer initialized
[ 0.220672] Bluetooth: SCO socket layer initialized
[ 0.220886] Switching to clocksource gp timer
[ 0.239471] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.239685] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[ 0.239868] MUSB0 controller's USBSS revision = 4ea20800
[ 0.240814] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using DMA, IRQ 18
[ 0.241149] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[ 0.241333] MUSB1 controller's USBSS revision = 4ea20800
[ 0.241821] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.241912] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.242065] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.242065] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.242095] usb usb1: Product: MUSB HDRC host driver
[ 0.242095] usb usb1: Manufacturer: Linux 3.2.0-00244-gcf99001 musb-hcd
[ 0.242095] usb usb1: SerialNumber: musb-hdrc.1
[ 0.242645] hub 1-0:1.0: USB hub found
[ 0.242675] hub 1-0:1.0: 1 port detected
[ 0.243072] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using DMA, IRQ 19
[ 0.243438] NET: Registered protocol family 2
[ 0.243652] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.244049] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.244201] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.244293] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.244323] TCP reno registered
[ 0.244323] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.244354] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.244567] NET: Registered protocol family 1
[ 0.244873] RPC: Registered named UNIX socket transport module.
[ 0.244873] RPC: Registered udp transport module.
[ 0.244903] RPC: Registered tcp transport module.
[ 0.244903] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.245178] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.361724] ashmem: initialized
[ 0.361999] VFS: Disk quotas dquot_6.5.2
[ 0.362060] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.362945] fuse init (API version 7.17)
[ 0.363189] msgmni has been set to 488
[ 0.364257] io scheduler noop registered
[ 0.364257] io scheduler deadline registered
[ 0.364349] io scheduler cfq registered (default)
[ 0.364959] Could not set LED4 to fully on
[ 0.366241] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.975646] console [ttyO0] enabled
[ 0.979705] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.987396] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.995056] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 1.002716] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 1.010314] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 1.018127] [drm] Initialized drm 1.1.0 20060810
[ 1.028930] brd: module loaded
[ 1.035430] loop: module loaded
[ 1.038879] i2c-core: driver [tsl2550] using legacy suspend method
[ 1.045379] i2c-core: driver [tsl2550] using legacy resume method
[ 1.051818] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.111450] No daughter card found on AM335x EVM
[ 1.116333] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.131500] Board name: A335BONE
[ 1.134887] Board version: 00A6
[ 1.138153] The board is a AM335x Beaglebone.
[ 1.144470] tps65217 1-0024: TPS65217 ID 0xf version 1.1
[ 1.151855] print_constraints: DCDC1: 900 <--> 1800 mV at 1800 mV
[ 1.160095] print_constraints: DCDC2: 900 <--> 3300 mV at 1275 mV
[ 1.168395] print_constraints: DCDC3: 900 <--> 1500 mV at 1125 mV
[ 1.176666] print_constraints: LDO1: 1000 <--> 3300 mV at 1800 mV
[ 1.184936] print_constraints: LDO2: 900 <--> 3300 mV at 3300 mV
[ 1.193115] print_constraints: LDO3: 1800 <--> 3300 mV at 3300 mV
[ 1.201385] print_constraints: LDO4: 1800 <--> 3300 mV at 3300 mV
[ 1.210876] Maximum current provided by the USB port is 500mA which is not sufficient
[ 1.210876] when operating @OPP120, OPPTURBO and OPPNITRO. The current requirement for some
[ 1.210876] use-cases using OPP100 might also exceed the maximum current that the
[ 1.210906] USB port can provide. Unless you are fully confident that the current
[ 1.210906] requirements for OPP100 use-case don't exceed the USB limits, switching
[ 1.210906] to AC power is recommended.
[ 1.255706] omap_hsmmc.0: alias fck already exists
[ 1.261016] omap_i2c.3: alias fck already exists
[ 1.281524] omap_i2c omap_i2c.3: bus 3 rev2.4.0 at 100 kHz
[ 1.289031] at24 3-0054: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.296325] IN : bone_setup_display_daughter_board
[ 1.341491] No display cape found on BeagleBone
[ 1.346618] da8xx_lcdc.0: alias fck already exists
[ 1.351928] da8xx_lcdc da8xx_lcdc.0: GLCD: Found Sharp_LCD035Q3DG01 panel
[ 1.366577] at24 3-0055: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.373870] IN : bone_setup_daughter_board
[ 1.431518] at24 3-0056: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.438781] IN : bone_setup_daughter_board
[ 1.501525] at24 3-0057: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.508789] IN : bone_setup_daughter_board
[ 1.571685] (hci_tty): inside hci_tty_init
[ 1.576141] (hci_tty): allocated 251, 0
[ 1.580291] NFC Driver for TI WiLink
[ 1.584777] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.591857] omap2-nand driver initializing
[ 1.596191] OneNAND driver initializing
[ 1.600708] CAN device driver interface
[ 1.604736] CAN bus driver for Bosch D_CAN controller 1.0
[ 1.651519] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.657989] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
[ 1.665466] davinci_mdio.0: probed
[ 1.669036] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720
[ 1.677642] PPP generic driver version 2.4.2
[ 1.682312] PPP BSD Compression module registered
[ 1.687225] PPP Deflate Compression module registered
[ 1.692626] usbcore: registered new interface driver cdc_ether
[ 1.698791] usbcore: registered new interface driver cdc_eem
[ 1.704742] usbcore: registered new interface driver dm9601
[ 1.710632] usbcore: registered new interface driver cdc_subset
[ 1.716857] cdc_ncm: 04-Aug-2011
[ 1.720275] usbcore: registered new interface driver cdc_ncm
[ 1.726287] usbcore: registered new interface driver cdc_acm
[ 1.732208] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 1.740539] Initializing USB Mass Storage driver...
[ 1.745819] usbcore: registered new interface driver usb-storage
[ 1.752075] USB Mass Storage support registered.
[ 1.757049] usbcore: registered new interface driver usbserial
[ 1.763214] USB Serial support registered for generic
[ 1.768524] usbcore: registered new interface driver usbserial_generic
[ 1.775360] usbserial: USB Serial Driver core
[ 1.779937] USB Serial support registered for GSM modem (1-port)
[ 1.786376] usbcore: registered new interface driver option
[ 1.792205] option: v0.7.2:USB Driver for GSM modems
[ 1.799011] gadget: Mass Storage Function, version: 2009/09/11
[ 1.805206] gadget: Number of LUNs=1
[ 1.809051] lun0: LUN: removable file: (no medium)
[ 1.814392] gadget: android_usb ready
[ 1.818328] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 1.823944] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[ 1.831787] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 1.838867] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 1.846405] usb usb2: Product: MUSB HDRC host driver
[ 1.851593] usb usb2: Manufacturer: Linux 3.2.0-00244-gcf99001 musb-hcd
[ 1.858489] usb usb2: SerialNumber: musb-hdrc.0
[ 1.863739] hub 2-0:1.0: USB hub found
[ 1.867675] hub 2-0:1.0: 1 port detected
[ 1.872467] mousedev: PS/2 mouse device common for all mice
[ 1.879455] using rtc device, am33xx-rtc, for alarms
[ 1.884552] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
[ 1.891784] am33xx-rtc: already running
[ 1.895812] i2c /dev entries driver
[ 1.899780] Linux video capture interface: v2.00
[ 1.904937] usbcore: registered new interface driver uvcvideo
[ 1.910949] USB Video Class driver (1.1.1)
[ 1.918182] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.924743] device-mapper: uevent: version 1.0.3
[ 1.929748] device-mapper: ioctl: 4.22.0-ioctl (2011-10-19) initialised: dm-devel@redhat.com
[ 1.938598] Bluetooth: HCI UART driver ver 2.2
[ 1.943237] Bluetooth: HCI H4 protocol initialized
[ 1.948242] Bluetooth: HCILL protocol initialized
[ 1.953155] Bluetooth: Bluetooth Driver for TI WiLink - Version 1.0
[ 2.035552] cpuidle: using governor ladder
[ 2.040069] cpuidle: using governor menu
[ 2.046997] usbcore: registered new interface driver usbhid
[ 2.052917] usbhid: USB HID core driver
[ 2.057647] logger: created 256K log 'log_main'
[ 2.062591] logger: created 256K log 'log_events'
[ 2.067718] logger: created 256K log 'log_radio'
[ 2.072784] logger: created 256K log 'log_system'
[ 2.078460] usbcore: registered new interface driver snd-usb-audio
[ 2.086364] ALSA device list:
[ 2.089477] No soundcards found.
[ 2.093109] oprofile: hardware counters not available
[ 2.098419] oprofile: using timer interrupt.
[ 2.103149] Netfilter messages via NETLINK v0.30.
[ 2.108245] nf_conntrack version 0.5.0 (3906 buckets, 15624 max)
[ 2.115020] ctnetlink v0.93: registering with nfnetlink.
[ 2.120697] NF_TPROXY: Transparent proxy support initialized, version 4.1.0
[ 2.128082] NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
[ 2.134643] xt_time: kernel timezone is -0000
[ 2.139556] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 2.145446] arp_tables: (C) 2002 David S. Miller
[ 2.150390] TCP cubic registered
[ 2.154083] NET: Registered protocol family 10
[ 2.159759] Mobile IPv6
[ 2.162445] ip6_tables: (C) 2000-2006 Netfilter Core Team
[ 2.168395] IPv6 over IPv4 tunneling driver
[ 2.173675] NET: Registered protocol family 17
[ 2.178405] NET: Registered protocol family 15
[ 2.183135] can: controller area network core (rev 20090105 abi 8)
[ 2.189819] NET: Registered protocol family 29
[ 2.194519] can: raw protocol (rev 20090105)
[ 2.199005] can: broadcast manager protocol (rev 20090105 t)
[ 2.205627] Bluetooth: RFCOMM TTY layer initialized
[ 2.210784] Bluetooth: RFCOMM socket layer initialized
[ 2.216247] Bluetooth: RFCOMM ver 1.11
[ 2.220184] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.225799] Bluetooth: BNEP filters: protocol multicast
[ 2.231323] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.237731] Registering the dns_resolver key type
[ 2.242797] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 2.250885] ThumbEE CPU extension supported.
[ 2.255462] mux: Failed to setup hwmod io irq -22
[ 2.261352] Power Management for AM33XX family
[ 2.266296] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 2.273071] Copied the M3 firmware to UMEM
[ 2.277465] Cortex M3 Firmware Version = 0x181
[ 2.286834] clock: disabling unused clocks to save power
[ 2.294342] Detected MACID=0:18:31:8e:53:6e
[ 2.300415] omap_rtc am33xx-rtc: setting system clock to 2000-01-01 00:00:44 UTC (946684844)
[ 2.310089] Waiting for root device /dev/mmcblk0p2...
[ 2.352691] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 2.363739] mmc0: new high speed SDHC card at address 1234
[ 2.370147] mmcblk0: mmc0:1234 SA04G 3.63 GiB
[ 2.377319] mmcblk0: p1 p2 p3 p4
[ 4.596435] EXT4-fs (mmcblk0p2): recovery complete
[ 4.604431] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 4.613098] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 4.620117] Freeing init memory: 344K
[ 4.656524] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
[ 4.770904] init: cannot open '/initlogo.rle'
[ 6.245086] EXT4-fs (mmcblk0p3): recovery complete
[ 6.254302] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,errors=panic
[ 6.325744] android_usb: already disabled
[ 6.342285] android_usb: already disabled
[ 6.347900] android_usb: already disabled
[ 6.353668] adb_bind_config
[ 6.359619] adb_bind_config
[ 6.503356] adb_open
root@android:/ # [ 6.750183] android_work: sent uevent USB_STATE=CONNECTED
[ 6.756072] android_work: sent uevent USB_STATE=DISCONNECTED
[ 6.791778] warning: `rild' uses 32-bit capabilities (legacy support in use)
[ 6.860076] android_work: sent uevent USB_STATE=CONNECTED
[ 6.867034] gadget: high-speed config #1: android
[ 6.873474] android_work: sent uevent USB_STATE=CONFIGURED
[ 12.544860] request_suspend_state: wakeup (3->0) at 12512097850 (2000-01-01 00:00:54.739846601 UTC)
[ 19.731201] request_suspend_state: wakeup (0->0) at 19698468701 (2000-01-01 00:01:01.926217452 UTC)
[ 27.998291] request_suspend_state: wakeup (0->0) at 27965558542 (2000-01-01 00:01:10.193276776 UTC)
[ 30.243164] request_suspend_state: wakeup (0->0) at 30210431590 (2000-01-01 00:01:12.438180341 UTC)
.......
The last line repeats .... I changed loglevel in init.rc to 1 .by default it was 3..
Can anybody help me to resolve this issue ...I am using ubuntu 10.04 64 bit as my host system and usb powering the board ..