Other Parts Discussed in Thread: OMAP3530
I'm looking at doing a "update" to one of my camera boards.
And use the OMAP3530 which seems idea for the application.
One of the issues is I need two "USB" high-speed ports. (And it would be
nice to keep the OTG port for debug/setup usage)
In the "briefs" it keeps refering to support for multiple ports on the HS
ie 1 USB 2.0 HS 3-Port,1 USB 2.0 HS OTG
Or is the 3-port comment off a bit. In which case I would need
a phy and a 2-port usb hub (I did some searching and having seen a combination of a PHY/HUB in one)