Other Parts Discussed in Thread: AM1808
For the AM1808 Power-On Sequence:
- The device should be powered-on in the order described in the datasheet.
- There is no specific required voltage ramp rate for any of the supplies as long as the LVCMOS supplies operated at 3.3V (DVDD3318_A, DVDD3318_B, or DVDD3318_C) never exceed the STATIC 1.8V supplies by more than 2 volts.
If the power supplies reach their nominal values in the order described in the datasheet, can the power supplies be powered-on at the same time?
Best regards,
Daisuke