This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP L138 VPIF

Other Parts Discussed in Thread: OMAP-L138

If I use VPIF at the OMAP L138, is it possible to encode the video to h.264 or MJPEG? Has the OMAP enough power to do this and which frame rate can I expect depending on the resolution?
Thanks for your help.

  • Hi Ralf,

    We do not have official numbers for h.264 and MPEG performance for OMAP-L13x yet.

    I will look into it and let you know if I find an estimation.

     

  •  

    HI Ralf,

    Here are some estimated numbers: 

    Test Case

    H264_DEC_3

    H264_DEC_4

    MPEG4_DEC_1

    MPEG4_DEC_2

    MPEG4_DEC_3

    MPEG4_DEC_4

    MPEG4_DEC_5

    Data Rate

    VBR, 4 Mbps

    VBR, 3 Mbps

    CBR, 1 Mbps

    CBR, 10 Mbps

    CBR, 300 Kbps

    VBR, 3 Mbps

    VBR, 2 Mbps

    Resolution

    D1

    VGA

    CIF

    D1

    QVGA

    VGA

    VGA

    FPS

    24.93

    35.21

    96.87

    33.69

    129.97

    52.25

    44.27

     

     

    H264_ENC_1

    H264_ENC_2

    H264_ENC_3

    H264_ENC_4

    H264_ENC_5

    Data Rate

    10 Mbps

    8 Mbps

    5 Mbps

    4 Mbps

    4 Mbps

    Resolution

    QVGA

    CIF

    VGA

    D1-NTSC

    D1-NTSC

    ChromaFormat

    4:2:0

    4:2:0

    4:2:0

    4:2:0

    4:2:2

    FPS

    39.2

    31.79

    14.57

    13.81

    12.97

     

    For MPEG 4 encoder:

    Number of channels 1
    Max resolution D1
    Max bit rate 5Mbps
    FPS 30 (see Comment)
    Profiles supported SP

    But these numbers were achieved reading and writting to a file, so you can expect a 10 - 20 % of decrease when using  the hardware.

     

  • If you are also interested in Motion JPEG ("If I use VPIF at the OMAP L138, is it possible to encode the video to h.264 or MJPEG?") then the JPEG Encoder is included with the SDK.

  • Hi Mariana,

     

    can you publish the sample code used for this performance estimation. I have a big problem to get MPEG4 encoder example (designed for C64+) running on L138 (DPS encoder only)?

     

    Thanks in advance

  • Hi

    Could you tell me how you performed the tests? Did you use the sample H264 and MPEG4 implementations that are present in the Codec Engine release for OMAP-L138?

    Regards
    Szymon