This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C66x AIF2 CPRI Single Tone Test



Hello,

I have compiled the single tone test for 66x keystone 2 device without any problems. However when I run the test in loopback mode I get the following results. Can anyone please guide me through this problem?

[C66xx_0] Beginning AIF2 LTE RF tests:
test: LTE_20MHZ_RF_SINGLE_TONE
AIF CPRI mode
link 0 runs at 4x rate
outbound data type: DL
outbound data width: 15 bit
inbound data type: DL
inbound data width: 15 bit
link 1 is disabled
link 2 is disabled
link 3 is disabled
link 4 is disabled
link 5 is disabled
Number of monolithic packets received in RX queue channel0: 0
Number of monolithic packets in TX free queue for channel0: 14
Number of monolithic packets received in RX queue channel1: 0
Number of monolithic packets in TX free queue for channel1: 14
Test a) Monolithic Packet Data Recv: on chan: 0 are :0
Test a) Monolithic Packet Data Send/Recv: FAIL
Test b1) Monolithic Packet Tx Descriptor Counts:0 PASS
Test b2) Monolithic Packet Tx Complete Descriptor Counts:28 PASS
Test b3) Monolithic Packet Rx Descriptor Counts:0 PASS
Test b4) Monolithic Packet Rx Free Descriptor Counts:0 FAIL

######### AIF2 ERRORS ###########
PE link0:2 DB did not have antenna data for a AxC channel. Likely to occur if DMA was late.

######### AIF2 INFO ##############
DB:637 Ingress FIFO buffer channel overflowed. This can happen if the AIF2 VBUSM interface is stalled by the system. This is not a fatal error. The AIF2 can gracefully recover from this condition

###############################

Ending LTE_20MHZ_RF_SINGLE_TONE test
Test: ending AIF2 LTE 20Mhz RF test
Some tests have failed
End of Program!!