Hi --
I sort of asked this question in a previous post, but you had to read through my evolving thought process to get to it. So here it is on its own. Anybody have any idea the best peripheral to use to transfer data from an external device via PCI Express? I'm thinking conceptually of having a PCI Express endpoint manager on a card that connects as directly as possible (don't know what logic, if any, might need to sit in between) to the OMAP-L138 board. From the OMAP-L138 board's persepective, what is the best interface to use to transmit/receive as high-speed as possible (a full 16 lanes of PCIExpress is capable of transferring 5GB/sec) data via a PCIExpress connection to another host processor.
If anybody has any thoughts onthis, I would love to hear them.
Thanks.
Mike