One by one,
TMDXEVM6678LE: Rev 3B
CCS5.4, NDK in MCSDK 2.1.2.6 , HUA test case,
100MB data from windows machine.
The TCP throughput is about 271Mb/s while UDP is 152 Mb/s
EVMK2HX: Rev11
CCS5.4, mcsdk_linux_3_00_01_12, linux and iperf to a linux x64 host
0.0-10.0 sec 236 Mb/s on TCP
If I test between two x64 machines, the bandwidth is above 900Mb/s, so our network system should be good.
We actually test several boards we have and they all behave similar.
I wonder if there is that our test problem or the platform issue.
Thanks