This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X custom board resistive touch panel(7 inch) not working in Android



Hi,

My ADC connections are exactly like EVM settings. I am able to get the touch events once after complete JB boot.But gui not taking the touches.

In board-am335xevm.c file the Max and min parameters are hard coded. is there any thing else i need to modify apart from this. My resistive touch panel(7 inch) is different make from what it is used in EVM.

To build the source code I am using starter kit command. Is that making GUI not works because starter kit uses 4.3 inch RTP?

Kindly help me

Regards,

Chandra