This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385 DCC AWB Problem

Other Parts Discussed in Thread: DM385

I'm using DCC for DM385 Image tuning. (ImageTuningTool_Version1.0.0 (DCCSetup_Lite.exe,  build Ver 2.0.4)).

I have a problem in AWB step.

Input raw data & Click 4 positions.

then in “Tuning Para Data” Tab, Click  “Next Page” button.

DCC error occurs below message.

Plugin returned message:
No flash has not yet been tuned, default params loaded.
Please load all reference files for No flash, then go to the next step.

H3A Info:Failed to generate config file! Command line used was:
h3a.exe "C:\DCC\Ex0\.plugoutdir\DC_AWB\h3a_temp.cfg" 1920 1080 36 128

I can't go next step.

please, help me.^^