Hello,
I have a question for the features supported by AM335x drivers.
I think that the supported features are described at the following page.
http://processors.wiki.ti.com/index.php/AM335x-PSP_04.06.00.10_Features_and_Performance_Guide
I found that "Auto negotiation", "Full duplex and half duplex mode of operation" ... are supported.
However, I can't find whether "flow control" is supported.
Is "Flow control" supported?
If it's not supported, how can I support the "Flow control" feature?
I think that it's described at "14.3.2.12 Flow Control" in TRM.
Best Regards.
Nomoto