This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

L138 USB0_VDDA33 Supply

Hi

I have a L138 application where all the DVDD IO voltages are powered by 1.8v and Core/PLL at 1.2v.

This design also uses Li-Ion batteries.

Can I turn off my 3.3v regulator, powering only the USB0_VDDA33 supply when USB module is turned off and not in use?

This will eliminate the need for a buck boost regulator just for USB, and I can source the supply from the USB 5v port itself.

  • Would you please share with me your power-up, power-down sequence? If not using the buck boost regulator to supply 3.3V to USB0_VDDA33, how do you plan to supply 3.3V from the 5V VBUS?

    Thanks

    David

  • Hi

    Attached is the power management tree.

    As you can see, the power regulator is a switching buck regulator that provides the 1.2v and 1.8v to the L138.

    The power up sequence is from the lowest, then highest, i.e. 1.2v first then 1.8v.

    If there is a need for USB communication, only then upon plugging in from the computer USB hub, the 5V external would provide another 3.3v LDO to source the USB_VDD33 to OMAP.

    Is this okay.

  • Hi, anybody from TI can comment on this implementation?

    The documentation does state that if the USB0 module is being turned off, the supplies can be removed; but I wanted to make sure no issues with this.

  • Hi Faisal

    We discussed this internally, and unfortunately the way you are trying to use , is not the intended use-case.

    We only support USB 1.8 and 3.3V being off together (as would be the use-case when users are not using USB0 in their design). We cannot recommend just turning portion of the USB PHY power for extended period of time or otherwise, as there is no in-built isolation to allow one of the supplies to be turned off etc.

    Regards

    Mukul