Has anyone been able to NFS mount a rootfs over usbnet on am335x? I have been able to get the SPL and u-boot to boot over USB. I have the USB gadget driver and ethernet support statically built into the kernel. When the kernel boots, I can see the eth0 on the host, but not on the beaglebone. I can manually bring up the usb0 on beaglebone and manually assign an IP address, but cannot ping it.
Platform beaglebone black.
ti-sdk-am335x-evm-06.00.00.00
Ubuntu 10.04 guest on VMware
regards -emil