Hi,
I am using a custom board based on AM3517. I need to control the brightness of the LCD through a UI application. I have done the coding for the brightness control through PWM and I am able to see some changes while setting duty cycle from 10% to 90%. But the difference in brightness(from 10% to 90%) is not good enough. Also, the brightness set at 90% is also not very high. I am using vxworks OS.
PFA is the code snippet which I am using to control the brightness. Can anyone tell me where I am going wrong? How can I increase the brightness seen on the LCD?
#define CM_FCLKEN1_CORE_ADDR 0x48004a00 #define CM_ICLKEN1_CORE_ADDR 0x48004a10 /* Control register */ #define CONTROL_PADCONF_START 0x48002030 /* MUX register */ #define GPT11_MUX_OFFSET (0x480021DC - CONTROL_PADCONF_START) #define PWM_ENABLE_MUX 0x0001 /* Clock register */ #define CLOCK_CONTROL_REG_CM_START 0x48004A00 #define CM_CLKSEL_CORE_OFFSET 0x40 /* GPT11 register */ #define GPT11_CTL_BASE 0x48088000 /* GPT register offsets */ #define GPT_TIOCP_CFG 0x010 #define GPT_TISTAT 0x014 #define GPT_TCLR 0x024 #define GPT_TCRR 0x028 #define GPT_TLDR 0x02C #define GPT_TTGR 0x030 #define GPT_TMAR 0x038 #define GPT_TSICR 0x040 /*This register controls optional features specific to the timer functionality*/ /* TCLR bits for PWM */ #define GPT_TCLR_ST (1 << 0) /* stop/start */ #define GPT_TCLR_AR (1 << 1) /* one shot/auto-reload */ #define GPT_TCLR_CE (1 << 6) /* disable/enable compare */ #define GPT_TCLR_TRG_OVFL_MATCH (2 << 10) /* trigger on overflow and match */ #define GPT_TCLR_PT (1 << 12) /* pulse/toggle modulation */ /*// bitmask defines for TIOCP_CFG*/ #define EMUFREE (0x00000020) /*// bit 5*/ #define SOFTRESET (0x00000002) /*// bit 1*/ /*// bitmask defines for TSICR*/ #define SFT (0x00000002) /*// bit 1*/ /*OVF_Rate = (0xFFFF FFFF - GPTn.TLDR + 1) * (timer-functional clock period) * PS For TLDR = 0xFFFFFF00 and PS=1(as no prescaler used) with clk=32kHz the OVF_Rate = 8ms */ #define DEFAULT_TLDR 0xFFFFFE00 /*TLDR : The value of the timer load register*/ /* default 50% duty cycle */ #define DEFAULT_DUTY_CYCLE 50 #define DEFAULT_TMAR (DEFAULT_TLDR + (0xFFFFFFFF - DEFAULT_TLDR - 1) * DEFAULT_DUTY_CYCLE / 100) /* default TCLR is off state */ #define DEFAULT_TCLR ( GPT_TCLR_PT | GPT_TCLR_TRG_OVFL_MATCH | GPT_TCLR_CE | GPT_TCLR_AR ) void udAm35xxLcdPwmSetDutyCycle(unsigned int duty_cycle1) { uint32_t tldr, tmar, tclr; uint32_t new_tmar; tldr = DEFAULT_TLDR; /*TLDR : The value of the timer load register.*/ new_tmar = (duty_cycle1 * num_settings) / 100; if (new_tmar < 1) new_tmar = 1; else if (new_tmar > num_settings) new_tmar = num_settings; tmar = tldr + new_tmar; UGL_AM35XX_WRITE_REG32(GPT11_CTL_BASE + GPT_TMAR, tmar); UGL_AM35XX_WRITE_REG32(GPT11_CTL_BASE + GPT_TCRR, tmar); udAm35xxLcdPwmEnableClock(); tclr = DEFAULT_TCLR; tclr |= GPT_TCLR_ST; UGL_AM35XX_WRITE_REG32(GPT11_CTL_BASE + GPT_TCLR, tclr); } void udAm35xxLcdPwmInit(void) { AM35XXSETBIT(CONTROL_PADCONF_START+GPT11_MUX_OFFSET, PWM_ENABLE_MUX); /*GPTIMER 11 functional clock is enabled*/ AM35XXSETBIT(CM_FCLKEN1_CORE_ADDR, (0x01 << 12)); /*GPTIMER 11 interface clock is enabled*/ AM35XXSETBIT(CM_ICLKEN1_CORE_ADDR, (0x01 << 12)); /*CLKSEL_GPT11: source is CM_32K_CLK*/ AM35XXCLRBIT((CLOCK_CONTROL_REG_CM_START+CM_CLKSEL_CORE_OFFSET), (1 << 7)); uint32_t tldr, tmar, tclr; uint32_t new_tmar; /*******************Reset the timer registers***************/ AM35XXSETBIT(GPT11_CTL_BASE + GPT_TIOCP_CFG, SOFTRESET); while (!UGL_AM35XX_READ_REG32(GPT11_CTL_BASE + GPT_TISTAT)); AM35XXSETBIT(GPT11_CTL_BASE + GPT_TSICR, SFT); while (!UGL_AM35XX_READ_REG32(GPT11_CTL_BASE + GPT_TISTAT)); AM35XXSETBIT(GPT11_CTL_BASE + GPT_TIOCP_CFG, EMUFREE); /***********************************************************/ /*Clear timer load and timer trigger registers */ UGL_AM35XX_WRITE_REG32(GPT11_CTL_BASE + GPT_TLDR, 0); UGL_AM35XX_WRITE_REG32(GPT11_CTL_BASE + GPT_TTGR, 0x1); tldr = DEFAULT_TLDR; tclr &= ~GPT_TCLR_ST; UGL_AM35XX_WRITE_REG32(GPT11_CTL_BASE + GPT_TCLR,tclr ); num_settings = 0xFFFFFFFE - tldr; UGL_AM35XX_WRITE_REG32(GPT11_CTL_BASE + GPT_TLDR, tldr); udAm35xxLcdPwmSetDutyCycle(DEFAULT_DUTY_CYCLE); }
Thanks & regards,
Shweta