Hi,
I try to optimize codes on DA830 platform. First, I use simulator C674x CPU Cycle Accurate Simulator to calculate the MCPS using Profile. But when I run the code on the hardware, the mcps is much high than that on simulator. I find that C674x CPU Cycle Accurate Simulator is flat memory. So I try to use simulator C6747 Device Cycle Accurate Simulator. The value is higher than hardware. If I want to use this simulator, how can I set this simulator? Except cmd file, should I use other gel file rather than the defualt one? Thanks!