Other Parts Discussed in Thread: OMAP-L137
Using OMAP-L137, I have DMA channel 8 performing a DMA memory-to-memory transfer. The associated IPR bit is set when the transfer completes. (I can poll for completion successfully.)
I am now trying to tie the same transfer to an interrupt. I already have an interrupt working on HWI7 for a GPIO input.
I have now tried mapping HWI6 to event 8, which I believe is the Transfer Completion interrupt. When that didn't work, I tried HWI8 and HWI7. In all cases, the GPIO interrupt continued to work (even when it was switched to HWI8).
Although I can still poll IPR for completion successfully, the ISR is not entered. See various snippets below.
server.tcf:
/* Currently, HWI7 is the DMA interrupt */
bios.HWI.instance("HWI_INT7").interruptSelectNumber = 8;
bios.HWI.instance("HWI_INT7").fxn = prog.extern("SPI_DMA_tcc_intr");
bios.HWI.instance("HWI_INT7").useDispatcher = 1;
bios.HWI.instance("HWI_INT7").interruptMask = "all";
/* Currently, HWI8 is the GPIO input interrupt */
bios.HWI.instance("HWI_INT8").interruptSelectNumber = 65;
bios.HWI.instance("HWI_INT8").fxn = prog.extern("MSI_ctl_intr");
bios.HWI.instance("HWI_INT8").useDispatcher = 1;
bios.HWI.instance("HWI_INT8").interruptMask = "all";
ISRs:
void MSI_ctl_intr()
{
SEM_postBinary(&SEM_MSIready);
}
void SPI_DMA_tcc_intr()
{
MCKINLEY_LED_setall((UInt16)(0x8)); //lights an LED
SEM_postBinary(&SEM_collect);
}
Interrupt setup:
C64_clearIFR(C64_EINT7|C64_EINT8);
C64_enableIER (C64_EINT7|C64_EINT8);
DMA setup:
#define CollectionDMA 8
bcnt = 1000;
acnt = 2;
pParam[0] = (0x00900000 | (CollectionDMA << 12));
pParam[1] = (UInt32)(&FakeData[0]); //Source
pParam[2] = (bcnt<<16)+acnt;
pParam[3] = (UInt32)dstPtr; //Destination
pParam[4] = (acnt<<16) + acnt; //In the memory to memory copy, but indices are 2 (same as acnt).
pParam[5] = 0xFFFF;
pParam[6] = 0;
pParam[7] = 1;
*icr = (0x01 << CollectionDMA);
*secr = 0xFFFFFFF;
*eesr = (0x01 << CollectionDMA);
*iesr = (0x01 << CollectionDMA);
*esr = (0x01 << CollectionDMA);
where icr, secr, eesr, iesr, and esr are pointers to the associated EDMA registers. The data is transferred. The appropriate IPR bit is clear before triggering the transfer and set after timing out SEM_pendBinary. I am not using a shadow region. Both the source and destination buffers are plenty large enough to hold the data.
I've tested the LED and, using the same call, I can light it in the background task or the GPIO input ISR. I'm pretty sure that I'm not getting the TCC interrupt, but I don't know why. The code is identical to the polled version except that I've added the interrupt enable and the write to *iesr. What more do I need to do to get the interrupt?