This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BBB devicetree timings and fbset

We are configuring a 16 bpp lcd panel.  The display is very close to looking perfect, we have a few artifacts that are mucking it up.

I had thought our dts file was looking good, but running fbset has made me second guess that.

If I change clock-frequency, hactive, or vactive and reboot I can see those changes have an affect.  However every time I run fbset gives me the following:

mode "640x480-0"
        # D: 0.000 MHz, H: 0.000 kHz, V: 0.000 Hz
        geometry 640 480 640 480 16
        timings 0 0 0 0 0 0 0
        accel true
        rgba 5/11,6/5,5/0,0/0
endmode

I'm concerned the following lines don't appear to have values set:  

# D: 0.000 MHz, H: 0.000 kHz, V: 0.000 Hz

timings 0 0 0 0 0 0 0

I'm thinking this might be a clue to the source of our artifacts, should I be concerned about?  Or am I on the wrong path?

Thanks

Below is the section from the dts file, I can include the whole dts file if needed.

device tree

			panel {
				compatible = "tilcdc,panel";
				pinctrl-names = "default";
				pinctrl-0 = <&jamex_lcd_pins>;
				panel-info {
					ac-bias           = <255>;
					ac-bias-intrpt    = <0>;
					dma-burst-sz      = <16>;
					bpp               = <16>;
					fdd               = <0x80>;
					tft-alt-mode      = <0>;
					stn-565-mode      = <0>;
					mono-8bit-mode    = <0>;
					sync-edge         = <0>;
					sync-ctrl         = <1>;
					raster-order      = <0>;
					fifo-th           = <0>;
					invert-pxl-clk;
				};

				display-timings {
					native-mode = <&timing0>;
					timing0: 640x480-63 {
						hactive         = <640>;
						vactive         = <480>;
						hback-porch     = <46>;
						hfront-porch    = <97>;
						hsync-len       = <2>;
						vback-porch     = <33>;
						vfront-porch    = <11>;
						vsync-len       = <2>;
						clock-frequency = <40000000>;
						hsync-active    = <1>;
						vsync-active    = <0>;
					};
				};
			};