I'm planning to drive a relay through a GPIO output from starter kit. This Relay requires input voltage of 5V for its coil. As main input supply (5V / 3A) is given to the starter kit, can I take 5V from Vbat & use to drive the relay.
If I need to increase the number relays to be driven, How can I calculate the voltage / current consumption in the starter kit design for each input & output.
Also from the starter kit design, I would like to know the spare GPIO pins available that I can use to drive the relays.