Design Objective
1. Sitara processor execute directly firmware from external parallel nor flash, therefore, external SDRAM is not needed, many costs can be saved.
2. The firmware executed from external parallel nor flash, includes TCP/IP stack. and Sitara ethernet switch function can be run normally.
Question
1. What kind of RTOS can support this kind of requirment?
2. If Linux OS can be used, what's the basic requirment to Hardware?