Hi all,
I 'm working on dm8107 which is a custom board.
When I set DDR3 working at 400MHZ,It can work well
But When I set DDR3 working at 533MHZ,we can enter linux system.
while the rdk demo can only run about several minutes and then the board would crash
In both cases the ARM clock is 720MHZ,HDVPSS and L3 is 240MHZ,ISS is 480MHZ, IVA is 390MHZ.
My DDR3 is 256MB and the bus width is 16bit
the rdk demo is a network-vdec-vdis demo