Other Parts Discussed in Thread: OMAPL138
Also, why am I getting "(AIS Parse):" for the output? I did not intend to use AIS. Is there something else using that in the background?
mono ./OMAP-L138/GNU/sfh_OMAP-L138.exe -p /dev/ttyUSB0 -targetType OMAPL138 -flashType NOR -flash_noubl /srv/tftp/u-boot.bin
-----------------------------------------------------
TI Serial Flasher Host Program for OMAP-L138
(C) 2012, Texas Instruments, Inc.
Ver. 1.67
-----------------------------------------------------
[TYPE] Single boot image
[BOOT IMAGE] /srv/tftp/u-boot.bin
[TARGET] OMAPL138
[DEVICE] NOR
[NOR Block] 0
Attempting to connect to device /dev/ttyUSB0...
Press any key to end this program at any time.
(AIS Parse): Read magic word 0x41504954.
(AIS Parse): Waiting for BOOTME... (power on or reset target now)
(AIS Parse): BOOTME received!
(AIS Parse): Performing Start-Word Sync...
(AIS Parse): Performing Ping Opcode Sync...
(AIS Parse): Processing command 0: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 11592-Byte section to address 0x80000000.
(AIS Parse): Processing command 1: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 1032-Byte section to address 0x80002D48.
(AIS Parse): Processing command 2: 0x58535906.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Performing jump and close...
(AIS Parse): AIS complete. Jump to address 0x80000000.
(AIS Parse): Waiting for DONE...
(AIS Parse): Boot completed successfully.
Waiting for SFT on the OMAP-L138...